Telcos To Figure Large in IOT and Edge Computing Data Centers

August 30, 2016 Damien Wells

The world of telecommunications has changed dramatically over the last few decades with the advent of the internet, cellular networks and Cloud computing revolutionising the way we communicate with each other. Deregulation and the denationalisation of traditional state-owned Telcos has also helped to change the landscape but is there a future for the traditional Telco as the internet continues to evolve along a number of different paths?

At a recent data center conference I asked Arun Shenoy, the Vice President of Schneider Electric’s IT business in the UK and Ireland, why he thought telecoms companies were likely to figure large in the Internet of Things (IoT) and Edge computing. See the video of our interview here.

“The evolution of the internet over the last 20 or so years has very much followed a consumption model,” he said. “In other words the end-user devices like mobile phones and smart phones of which there are about eight and a half billion in the world today, are really consumption devices. They pull content from what is ultimately a centralised location and that applies to streaming as much as it does to messaging or other applications.”

“As the internet develops to support the Internet of Things that consumption model is changing quite dramatically. We’re going to put sensors and actuators and other intelligent devices at the very edge of the network and instead of consuming content, they’re going to be producing content at which point in time the internet starts to freak a little bit because it was designed to be a consumption download mechanism, not a true bi-directional asynchronous platform.”

“So the choices that we have are actually quite simple: we can refurbish the internet infrastructure as a whole but that’s a very time-consuming, risk prone, expensive process or we can think a little bit differently about how we want to create data-centre infrastructure. I think that is where the market is moving and it is really moving in a couple of directions at the same time. In one sense it is moving towards the very large hyperscale data center players—the Amazons, Facebooks, Microsofts and Googles of this world who are essentially centralising large blocks of infrastructure to support the vast majority of Cloud requirements.”

“However, from an IoT perspective we need to understand that those devices are going to generate content and so we face a problem in terms of internet bottlenecks which will require a different solution. The market is going in two entirely complementary directions at the same time. It’s not a case of one or the other; it is a combination of both. That second area is the Edge and by that we mean a much larger highly distributed federated set of smaller data centres that are much closer to where the content is being created.”

“Now why is that important? The biggest driver from an IoT perspective is not coming from the consumer; it’s coming from industries such as water utilities, power stations, oil & gas, pharmaceuticals and factories. They are putting IoT devices in place so that they can better monitor and manage what is going on in their infrastructure. They want to use that intelligence to make very rapid decisions about how to automate infrastructure and how to be more energy and operationally efficient.”

“For those kinds of workload it is not optimal to take all the data back to the centre, process it and then send it all the way back to the Edge. It’s much more useful to do that in local loops and to do that you need to build local infrastructure.”

“Part of our development as an industry needs to take that into account. We talk about the life cycle of infrastructure, and nowhere is that more important than in Edge networks because we don’t have the luxury of developing and deploying Edge infrastructure if it remains a very human-intensive process to manage. So we have to use technology and automation so that we can better manage that remote infrastructure.”

“As the market develops in both directions, we at Schneider have a very clear view of what that future looks like and we have a set of product offerings, including software and automation platforms that can operate in both the hyper-scale space and at the Edge.”

“Telcos will have a strong play in this evolving landscape for a couple of reasons. Apart from the changes I already mentioned, there are other factors regulating this industry. Safe harbour and data sovereignty, for example, require a different model to a very centralised approach in which people are not quite sure where their data is being held.”

“For the last hundred years or so, Telcos have built their business entirely on that model. For example, when you pick up your mobile phone to make a call you don’t’ have to re-authenticate yourself with the network. There is already a relationship of trust between your device and the infrastructure because the Telcos have put in place systems to do just that. The challenge for them is that the consumption model is changing. It is no longer just about voice and data, it’s about rich applications; it’s about Cloud and it’s about content from both a creation and a consumption point of view.”

“So the Telcos have an infrastructure that is trusted, secure and reliable but it is not necessarily the right infrastructure to support an ICT workload. They will have to go through their own infrastructure modernisation programmes to move from a traditional telecoms network-switching driven environment to a much more converged ICT environment. In that way they can become part of the content-driven Cloud economy and develop applications and services that consumers want from them.”

“I don’t think they are going to go down the centralised route because for decades they built an infrastructure that suits them and their customers. I think they will simply modernise that infrastructure and that’s where Edge comes in for them. It’s that conversion from one architecture to another specifically so that they can participate in these much bigger opportunities.”

“There is going to be a huge increase in the amount of data generated over the internet and Telcos will be a vital element in enabling that to happen. We are going to move very quickly from 8bn connected smart phones to 20bn. About 50% of Chinese citizens are already on the internet and I saw a recent study that said that every Chinese citizen by 2020 will have seven IP addresses on their body. So you know we’re going to this highly connected world before we even get into the IoT space.”

“I think Telcos are the organisations that are best placed to leverage what they already have and modernise it. The cost of getting into that kind of infrastructure for companies that are not Telcos is huge and I think for the vast majority of them it will be incredibly prohibitive. So I strongly believe that Telcos are well placed to take advantage of the IoT and Edge Computing.”


The post Telcos To Figure Large in IOT and Edge Computing Data Centers appeared first on Schneider Electric Blog.


Previous Article
How DCIM Fits in Every Data Center
How DCIM Fits in Every Data Center

In any walk of life, you don’t want to take a sledge hammer to crack a nut, or as my colleagues in some par...

Next Article
The case for Design PUE Curve
The case for Design PUE Curve

As I get older, I have found I more easily get frustrated.   This is not good news since I want to avoid tu...


Ready to talk to an expert? Fill out your info and we'll be in touch:

First Name
Last Name
Company - optional
Would you like to sign up for our newsletter?
Phone Number
Country or region
Comments - optional
I am a
Thank you!
Error - something went wrong!

Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!