Battle of the UPSs

July 12, 2016 Patrick Donovan

A quantitative showdown between DRUPs and Static UPSs


Diesel rotary UPS (DRUPS) systems have found a niche in the data center industry as a backup power source for critical IT and cooling loads.  This technology of combining flywheel (or battery) energy storage with a diesel generator in one unit has been around for a long time.  The basic idea is that when utility power is lost, the flywheel or battery powers the load just long enough (seconds) for the diesel generator to come online to ensure continuous operation of the load.  This is positioned by some as a superior alternative to stand alone Static UPSs (paired with standby generators) more commonly used in data centers today.  Claims are often made that DRUPS is more efficient, uses “40-60% less space”, and is equally scalable as any other modular UPS.  But is this really true?  Or is this the same old bag of tricks that some marketers use to conjure value where there is none?

The answer (which is “same old tricks”) lies in the assumptions of the analysis, of course.  In this case, these misleading comparisons are apparently based on ancient UPSs with embarrassing efficiency curves, Static UPSs being saddled with way more battery runtime than necessary, and individual components being compared while ignoring the performance of the larger overall system.  So our “Center of Excellence” engineering team in Singapore responded with their own analysis; an analysis that is quantitative and based on real world conditions with published assumptions for all to see.  This analysis is now available for free in our new White Paper 222, “Diesel Rotary UPS (DRUPS) vs. Static UPS: A Quantitative Comparison for Cooling and IT Applications”.

Don’t have time to read the paper? Like with all of our white papers, you can always just read the exec summary and scan through the tables, figures, and end with the conclusion.  It’s a quick way to get the gist.  For this comparison, however, I can say right here that a Static UPS system (includes gensets, all the switchgear, batteries, thermal buffer tank, etc) in a common “2N” architecture is cheaper, more efficient, and has a lower 10 year TCO (about 7% less) than a comparable DRUPs system.  The Static UPS does, however, take up a bit more space…but is nowhere near the 40% savings claimed by some.  See the paper for all the details.  And we also analyzed the systems in a tri-redundant architecture as well in the Appendix.

The post Battle of the UPSs appeared first on Schneider Electric Blog.

Previous Article
Securing Power and Control: The Problem and Attack Vectors
Securing Power and Control: The Problem and Attack Vectors

Electricity is taken for granted. Lights illuminate when we flip a switch. Turn up the thermostat and the h...

Next Article
Battle of the UPSs
Battle of the UPSs

A quantitative showdown between DRUPs and Static UPSs Diesel rotary UPS (DRUPS) systems have found a niche ...

Need power protection for YOUR home office or living room?

Find Your UPS

Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!