The interest of legal metrology for billing applications

September 9, 2016 Franck Gruffaz

As anyone, I have to pay for the electricity, the gas or the water I am consuming in my house. As anyone, I would be very angry if I am overcharged and very happy if I am undercharged, and it would be the opposite for my energy provider.

This is why the instruments measuring all this for billing purposes are covered by regulations.

The term grid-level billing is related to commercial transactions between utilities, energy providers, or states. The simpler term billing is related to a commercial transaction between an energy provider and an energy consumer (customer). Grid level billing and billing are both related to legal metrology.

Legal metrology usually applies to measuring instruments used in:

  • Commercial transactions (e.g. weight-price scales for retail stores, petrol pumps, water meters, etc.), when there is a need to protect both the buyer and the seller.
  • Operations concerning public health or safety (e.g. gas analyzers, tachographs, radar speed detectors, breathalyzers, etc.).

For more detailed information on legal metrology applications, refer to the following resources:

Billing meters (also known as revenue meters, electricity meters or utility meters) are covered by regulations such as MID (Measuring Instruments Directive, Directive 2014/32/UE) in Europe.

Standards and regulations applicable to billing are shown in Table 1.

Application Assessment Standards or Rules Methods Standards Product Standards
Any countries can define its own regulation and/or can refer to international documents, such as the IEC International standards or OIML guide IEC 62052-xx


OIML R46 (Organisation Internationale de la Métrologie Légale)
European regulation (MID = Measuring Instruments Directive)

Directive 2014/32/UE

WELMEC guides EN 50470-1

EN 50470-3

US regulation ANSI C12.1, ANSI C12.20
Australian regulation (NMI) NMI M-6
Indian regulation IS 16244, IS 15884, IS 13779, IS 14697
Chinese regulation JJG 596
Canadian regulation LBM-EG-07

Table 1 – Documents related to Legal metrology

For more information on measuring applications, check out the white paper, “Guide to energy measurement applications and standards.

For more information on IEC 61557-12, check out the white paper, “Guide to using IEC 61557-12 standard to simplify the setup of an energy measurement plan.”

For additional tools, resources and product information, please register for our dedicated Consulting Engineer portal site.

The post The interest of legal metrology for billing applications appeared first on Schneider Electric Blog.

Previous Article
A Cold Answer to High and Stringent Cooling Demands
A Cold Answer to High and Stringent Cooling Demands

Control panels house the electronics and computer brains of a system. That makes them critical to success o...

Next Article
Daytona International Gets Smart About Panelboards
Daytona International Gets Smart About Panelboards

It’s home to what’s been called the Great American Race for years but Daytona International Speedway handle...

Need power protection for YOUR home office or living room?

Find Your UPS

Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!