Funding the Unfunded: Energy Savings Performance Contracts for Federal Data Center Consolidation

March 17, 2016

Written by Miles Auvil

2013 marks the third year of the Federal Data Center Consolidation Initiative (FDCCI) and inches agencies closer to its shared 2015 deadline with the coinciding Presidential Memorandum; disposing of unneeded federal real estate.  The initiative itself has primarily been unfunded with the hopes that the consolidation of federal data centers would ultimately generate savings that would allow agencies to fund and move forward with additional consolidation plans.  2013, to say the least, has been the most challenging year thus far with shrinking budgets from appropriated funds and more specifically sequestration.  The topic of alternative funding gains renewed interest during these challenging times, but few in IT are aware of some of the available and proven contracts available to federal agencies.

Energy Service Companies (ESCO’s) and the Department of Energy have advocated the use ofEnergy Savings Performance Contracts (ESPC’s) for Data Centers.  A few projects have emerged in the past year, some of which are viewed as pilots, but we have yet to see wide scale adoption.  In light of FDCCI and the current fiscal environment a significant opportunity for IT is being missed.

ESPC’s allow federal agencies to conduct energy projects with no upfront capital costs, minimizing the need for Congressional appropriations.  The projects are designed and constructed in a manner that meets the agency’s needs and the ESCO arranges the necessary funding and guarantees that the improvements will generate energy cost savings sufficient to pay for the project over the term of the contract.

A large majority of federal agencies have utilized this contract to improve the performance of buildings, however, data centers have not been addressed in most of the past contracts.  The barriers to performing ESPC’s on data centers are easily solvable and the first step is to educate.

In a recent meeting with a federal CIO, I put the opportunity in the context of visualizing energy as an asset.  Every dollar saved on your energy bill can be leveraged into improving and/or consolidating data centers and implementing efficient IT.  In addition, education can dispel misnomers of what ESPC’s can be used for.  When speaking with federal IT managers and asking about their awareness of ESPC’s, their association generally relates to infrastructure improvements such as lighting, HVAC, etc., all of which are highly sought after benefits to an ESPC.  However, rarely, if ever, have the dots connected back to an IT project that provides energy or operational savings such as Virtual Desktop Infrastructure (VDI), server consolidation or server virtualization.  These examples are just a few of the IT projects that can drive not only energy savings, but operational savings as well.

I will often show a slide during presentations on the topic of energy savings in data centers.  It identifies the areas of savings potential as it relates to power consumption of a device as a percent of IT load.  The low hanging fruit in the data center (CRAC/CRAH, Chillers, UPS, PDU Transformers) tends to get the most agreement from the audience, but the top of the graph, and the only category that reflects 100% (the IT Load) is rarely acknowledged.

If Federal agencies hope to meet the goals of FDCCI, dispose of unneeded real estate and comply with energy and environmental legislation in a less than ideal fiscal environment, future ESPC’s must address data centers and include both infrastructure and IT.

Previous Article
Data Center Knowledge - Optimizing Energy Savings in Federal Data Centers
Data Center Knowledge - Optimizing Energy Savings in Federal Data Centers

Next Article
Blog - Powering the Data Center Through Storm Season: Solar Flares
Blog - Powering the Data Center Through Storm Season: Solar Flares

Storm season is coming — and while we often think about the effects a major storm, such as a hurricane, mig...

×

Ready to talk to an expert? Fill out your info and we'll be in touch:

First Name
Last Name
Company - optional
Would you like to sign up for our newsletter?
Phone Number
Country or region
Comments - optional
I am a
Thank you!
Error - something went wrong!