Why Do Home Electrical Fires Still Happen?

November 22, 2017 Romain Grand

Unless the power goes out, we don’t think much about the electricity coursing through the wires in its walls and ceilings. But your electrical system could be harboring problems that threaten both your property and your life. U.S. fire departments annually responded to 45, 210 home structure fires involving electrical failure or malfunction between 2010 and 2014, according the National Fire Protection Association (NFPA). These fires resulted in 420 deaths, 1,370 injuries, and $1.4 billion in direct property damage each year.

electrical fire

How electrical fires happen

Your home could be at risk whether it was built last century or last year. Fortunately, electrical fires are preventable if you know what risks to look for. Here are the most common culprits:

Old appliances: Appliances that don’t meet modern safety standards or that have frayed cords or damaged plugs are one of the biggest causes of home electrical fires. Older appliances draw more power than today’s outlets are built to handle, and damaged cords channel heat onto carpets, curtains, floors, and other combustible surfaces.

Faulty outlets and switches: Appliance that get intermittent power – such as lights flickering on and off – or that cause sparks when you plug them in can signal a problem with the outlet. The wiring in outlets and switches can loosen over time and pose a fire threat. Both should be checked yearly for looseness, breaks, and corrosion.

Light fixtures: Lamps and other lighting can pose a danger when the bulb’s wattage exceeds the fixture’s suggested limit. Lamps with cloth or paper shades or decorated with other combustible materials can start fires when that material heats up. Antique lamps and other older fixtures may have damaged wiring that make them susceptible to overheating.

Extension cords: While generally safe when used correctly, extension cords become dangerous when too many appliances are plugged into a single cord. This can overburden the outlet if it’s not designed to handle that load. Even when you plug in a single appliance, extension cords should always be used temporarily, never as a permanent solution.

Space heaters: Portable space heaters, particularly the type with heating coils, cause fires when they’re placed too close to curtains, clothes, bedding, rugs, and cloth covered furniture. The heat from the coils can easily ignites the adjacent flammable material.

Defective wiring: The average home today uses more electrical appliances than ever before: Refrigerators, air conditioners, washers and dryers are now sharing your electrical system with computers, video game consoles, TV streaming boxes, and other consumer electronics. If your home is more than 20 years old, the wiring may not be able to handle the added load and could overheat and ignite a fire.

Find out if you’re at risk

Electrical fire threats don’t announce themselves; you have to look for them. You can start by checking your home appliances and wiring for damage and other risk factors. In addition to replacing old or damaged appliances, we recommend consulting with a licensed electrician to make any necessary repairs or upgrades to your electrical system.

Learn more about electrical safety and how you can prevent home electrical fires.

The post Why Do Home Electrical Fires Still Happen? appeared first on Schneider Electric Blog.


Previous Flipbook
Identifying Power Quality Issues and Implementing Solutions
Identifying Power Quality Issues and Implementing Solutions

Don’t let hidden power quality issues wreak havoc on your operations. Implementing power quality solutions ...

Next Article
Not Your Father’s UPS: Latest Models Offer Improved Efficiency, Management, Batteries and More
Not Your Father’s UPS: Latest Models Offer Improved Efficiency, Management, Batteries and More

Uninterruptible power supply (UPS) technology has changed quite a bit over the past several years, with new...


Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!