Important features to look for when choosing the right Back-UPS

April 26, 2019 Kavita Manral

Back-UPS is a type of UPS that offers battery backup and guaranteed power. The device is capable of controlling any surges that occur in the electrical systems. The system might include air conditioners, wireless networks, computers, gaming consoles or any other electronic device. The electrical surges, voltage fluctuations, damaging surges and spikes are the primary reason why electrical devices breakdown.

Schneider Electric India offers a range of domestic and industrial UPS and Back UPS which offers the following features:

Reliable Battery:

  • Automatic Self Test: The battery runs an automatic self-test to detect the faults in the device. The test is done to detect if the battery needs to be replaced.
  • Battery Failure Notification: It generates a warning notification on fault analysis. This helps in running timely maintenance checks in the system and do a preventive check of all the components.
  • Intelligent Battery Management: The modern day UPS is capable of maximizing battery performance, life, and reliability through intelligent, precision charging.

Maximised Protection:

  • Battery and surge protected outlets: Back-UPS has a secure battery backup and protection setup that protects the hardware devices and critical data during dirty power or power outages, surges or spikes.
  • Exclusive Surge Outlets: The surge arrester protects secondary electronic devices from power surges without reducing the power supply to the battery to run primary electronics during an outage.
  • Safety-agency approved: The entire setup is made secure by testing the product for safety. These devices work under safety certification by agencies in collaboration with connected service provider and equipment only in the specified environment.

Easy to Manage and Operate:

  • LED status display: The display of UPS battery backup is easy to understand and read. The power status is specified with visual indicators that are easy to interpret.
  • Audible alarms: It has audible alarms that provide notify the household of the fluctuating utility power and UPS power conditions.

The post Important features to look for when choosing the right Back-UPS appeared first on Schneider Electric Blog.

Read more...

Previous Article
How data centres will breathe life into 5G
How data centres will breathe life into 5G

Originally published on CNBC. 5G is rolling out in select markets in 2019 and will gather pace over the nex...

Next Article
Results are in! Our Study Measuring the Different Levels of Data Center Air Containment
Results are in! Our Study Measuring the Different Levels of Data Center Air Containment

In an earlier blog I explained the problem with “percent leakage” in regards to air containment and I propo...

×

Ready to talk to an expert? Fill out your info and we'll be in touch:

First Name
Last Name
Company - optional
Would you like to sign up for our newsletter?
Phone Number
Country or region
Comments - optional
I am a
Thank you!
Error - something went wrong!
×

Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!