What applications are driving the move to the Edge?

May 27, 2016

Click here to learn more about data center solutions http://bit.ly/2pqbnma Leonard Francis, Associate Director of IT Operations at Weill Cornell Medical College, talks about how different departments on their campus have different needs based on what they are doing. Some departments like research and administration have a need for speed with data connection, intimacy of data and overall increased need for data processing. Recorded at Data Center Dynamics Enterprise 2016. View the full panel about Edge Computing: http://bit.ly/1Uf4Im1. Learn more about Solutions for Edge Computing: http://bit.ly/1WXQ6yF

Previous Video
What Does the Industry Have to Do to Be Successful on the Edge?
What Does the Industry Have to Do to Be Successful on the Edge?

Click here to learn more about data center design http://bit.ly/2owCXAC Todd Traver, VP IT Optimization and...

Next Video
Edge Applications
Edge Applications

Todd Traver, VP IT Optimization and Strategy at Uptime Institute, explains that applications are more porta...