What Does the Industry Have to Do to Be Successful on the Edge?

May 27, 2016

Click here to learn more about data center design http://bit.ly/2owCXAC Todd Traver, VP IT Optimization and Strategy at Uptime Institute, explains that we need to think thru the application holistically understanding what is included and impacted by moving to the edge. Enterprise and Facility folks need to work together to develop the overall plan of going to the edge. Recorded at Data Center Dynamics Enterprise 2016. View the full panel about Edge Computing: http://bit.ly/1Uf4Im1. Learn more about Solutions for Edge Computing: http://bit.ly/1WXQ6yF

Previous Video
Evaluating & supporting a move to the Edge
Evaluating & supporting a move to the Edge

Click here to learn more about micro data centers http://bit.ly/2pq8GAL and data center solutions http://bi...

Next Video
What applications are driving the move to the Edge?
What applications are driving the move to the Edge?

Click here to learn more about data center solutions http://bit.ly/2pqbnma Leonard Francis, Associate Direc...