Using PMDs (Power Metering & Monitoring Devices) to Measure and Manage Energy Costs

August 10, 2016 Franck Gruffaz

Electricity meters have been critical components in facility electrical design since utility customers began paying for the commodity. However, while traditional meters at service-entrance points provide utilities with the consumption data they need for billing, they aren’t very helpful for facility owners and managers, who are more interested in how electricity is used, once it enters the building. Now, power metering and monitoring devices (PMDs) can help meet a range of needs, from monitoring the accuracy of the utility’s revenue meter to … This post outlines three valuable applications for PMDs.

Bill auditing

Electric utility bills often are simply accepted, as is, but that can be a big mistake for facility owners and managers because revenue meters aren’t infallible. For example, rate tariffs established years ago might no longer be accurate, thanks to efficiency upgrades installed over time. Additionally, billing intervals might be too long or too short, which can skew demand charges. Even mistakes in the building owner’s favor can be expensive in the long run, because supply contracts can allow the utility to recover missed charges months or years after an error occurs. For a commercial building owner, this could mean costs aren’t recoverable if tenants have moved out.

Figure 1 illustrates the relationship of a PMD to the utility’s revenue meter in a bill-auditing (also called “shadow metering” or “shadow billing”) application. As the figure shows, the PMD in this application is installed in parallel with the utility meter to calculate an accurate “shadow bill” that includes all expected energy and demand charges. This bill can then be compared to the utility bill to identify any inconsistencies. Note that the data in this use remains facility-wide.

Figure 1

Figure 1

Cost allocation
Owners of multi-building campuses, industrial plants and other facilities with multiple cost centers can benefit from access to clear information on each operation’s energy use. For example, such verified data can help owners better allocate energy expenses against specific revenues, as well as aid in establishing benchmarks and tracking the impact of efficiency upgrades, over time.

As Figure 2 shows, PMDs in this application are installed for each cost center to be tracked. Software systems compile the data from the PMDs and main revenue meter to determine each cost center’s contribution (as a percentage) to the facility’s total monthly electricity bill.

Figure 2

Figure 2

Sub-billing (also called tenant metering)
Similar to their use for cost allocation, PMDs in this application can help building owners allocate electricity costs by use – in this case, by the use of individual tenants in a larger commercial office or retail facility. As shown in Figure 3, these costs are usually combined with those for other services in tenants’ monthly facility bills. PMDs complying with the International Electrotechnical Commission’s Standard 61557-12 can be used for sub-billing purposes, as permitted by local regulations.

Figure 3

Figure 3

Save

Save

Table 1 outlines the standards and regulations and regulations applicable to these applications.

Table 1

Table 1

Compliance to IEC 61657-12 is a minimum requirement for all billing, cost-allocation and sub-billing applications. For even greater assurance of durability and measurement accuracy, Schneider Electric recommends specifiers call for devices that have been third-party certified. Manufacturers of such “C-PMD” products undergo regular manufacturing audits to ensure product quality and the devices, themselves, are subject to testing to ensure they can stand up to rigors in the field. For additional tools, resources and product information, please register for our dedicated Consulting Engineer portal site.

Save

The post Using PMDs (Power Metering & Monitoring Devices) to Measure and Manage Energy Costs appeared first on Schneider Electric Blog.

Read more...

Previous Article
Talking Data Center Design Architecture with Digital Reality
Talking Data Center Design Architecture with Digital Reality

In the fourth of our “8 Megatrends” series, we sat down with Kevin Dalton, V.P Engineering, Digital Reality...

Next Flipbook
Galaxy VX Brochure
Galaxy VX Brochure

×

Become a Data Center Expert - get the latest content before anyone else

Thank you
Error - something went wrong!